:MEASure:HORizontal:BINTerval:UREFerence:VALue
Command Syntax
:MEASure:HORizontal:BINTerval:UREFerence:VALue <time_location>
<time_location> is a double.
Query Syntax
:MEASure:HORizontal:BINTerval:UREFerence:VALue?
Description
When a user-defined horizontal reference location is enabled (see :MEASure:HORizontal:BINTerval:UREFerence:STATe), this command specifies its time location with respect to the trigger (t = 0) location.