:MEASure:HORizontal:STIMe:CEDirection
Command Syntax
:MEASure:HORizontal:STIMe:CEDirection {RISing | FALLing | BOTH}
Query Syntax
:MEASure:HORizontal:STIMe:CEDirection?
Description
For the :MEASure:HORizontal:STIMe measurement, specifies which clock signal edges to consider in the measurement.
The BOTH option means both rising and falling clock signal edges are considered to be clock edges.
Example Command Sequence
This sequence sets up the measurement using both data signal edges and the falling clock signal edge.
:MEASure:HORizontal:STIMe:SOURce1 CHAN1_1
:MEASure:HORizontal:STIMe:SOURce2 CHAN1_2
:MEASure:HORizontal:STIMe:DEDirection BOTH
:MEASure:HORizontal:STIMe:CEDirection FALLing
// Perform measurement
:MEASure:HORizontal:STIMe
:MEASure:HORizontal:STIMe?