:MEASure:JITTer:JITTer:DDJ?
Query Syntax
:MEASure:JITTerN:JITTer:DDJ?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Description
Returns DDJ (p-p), the Data Dependent Jitter, the peak-to-peak (p-p) range of the jitter that is correlated to the data pattern.