:MEASure:JITTer:JITTer:PJRMs?
Query Syntax
:MEASure:JITTerN:JITTer:PJRMs?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Description
Returns PJ (rms), Periodic Jitter RMS, which is the root-mean-square value of the uncorrelated periodic jitter.