:MEASure:JITTer:JITTer:TJ:STATus?

Query Syntax

:MEASure:JITTerN:JITTer:TJ:STATus?

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Response

{CORR | INV | QUES}
CORR
The measurement result is correct.
INV
The measurement result is invalid.
QUES
The measurement result is questionable.

Description

Queries the status of the :MEASure:JITTer:JITTer:TJ? measurement. Use the :MEASure:JITTer:JITTer:TJ:STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :MEASure:JITTer:JITTer:TJ:STATus:DETails? child query.

See Also