:MEASure:JITTer:NOISe:COUNt?
Query Syntax
:MEASure:JITTerN:NOISe:COUNt?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Description
Returns the Bit Count, which is the number of symbols that have been measured. The value is returned for the level specified by :MEASure:JITTer:NOISe:COUNt:LEVel.