:MEASure:JITTer:NOISe:DI?
Query Syntax
:MEASure:JITTerN:NOISe:DI?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Description
Returns DI (δ-δ), Deterministic Interference, which is a measure of the amount of vertical interference on a signal due to deterministic causes. The value is returned for the level specified by :MEASure:JITTer:NOISe:DI:LEVel).