:MEASure:JITTer:NOISe:LEVel?

Query Syntax

:MEASure:JITTerN:NOISe:LEVel?

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Description

Returns the Level value measured for the level specified by :MEASure:JITTer:NOISe:LEVel:LEVel.

Level values are used in the calculation of other measurements like Eye Height (see :MEASure:JITTer:NOISe:EHEight?).