:MEASure:JITTer:NOISe:PIR:LEVel

Command Syntax

:MEASure:JITTerN:NOISe:PIR:LEVel {LEVel0 | LEVel1}

Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.

Query Syntax

:MEASure:JITTerN:NOISe:PIR:LEVel?

Description

This command specifies the level for which the measurement value is returned.