:MEASure:JITTer:NOISe:TI:LEVel
Command Syntax
:MEASure:JITTerN:NOISe:TI:LEVel {LEVel0 | LEVel1}
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Query Syntax
:MEASure:JITTerN:NOISe:TI:LEVel?
Description
This command specifies the level for which the measurement value is returned.