:MEASure:JITTer:NOISe:UIS?
Query Syntax
:MEASure:JITTerN:NOISe:UIS?
Where N identifies one of four possible jitter/noise analyses {1:4}. For example, JITTer4.
Description
Returns the number of Unit Intervals on which the noise measurements are based.