:MEASure:LLINe:FPOints:STATus?
Query Syntax
:MEASure:LLINeN:FPOints:STATus?
Where N identifies one of 64 {1:64} possible limit line tests. For example, :LLINe23.
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid.
- QUES
- The measurement result is questionable.
Description
Queries the status of :MEASure:LLINe:FPOints? query which returns the total number of failed data points in a specific Limit Line Test. Use the :MEASure:LLINe:FPOints:STATus:REASon? child query to determine the reason for an invalid or questionable measurement.