:MEASure:MARKer:DX?
Query Syntax
:MEASure:MARKer:DX{1:4}?
This command supports the STATus? and STATus:REASon? common child commands.
Description
Queries the difference in time between any two X-axis markers, whether they are tracking marker pair or manual line markers. The two markers can have different source waveforms. Use the :MARKer Subsystem to turn on markers. To display or hide the Δ Pos (delta position) and Δ Mag (delta magnitude) listings in the displayed Markers table, use the :DISPlay:MARKer:DELTas command.
Example Command Sequence
:MARKer:X1:SOURce CHANnel1 :MARKer:X2:SOURce CHANnel2 :MARKer:X1:STATe MANual// Marker 1 turned on as a manual line marker :MARKer:Y2A:STATe TRAC// Marker 2 turned on as a tracking marker pair … :MEASure:MARKer:DX2?