:MEASure:MHIStogram{N}:MEDian?
Query Syntax
:MEASure:MHIStogram{1:4}:MEDian?
Description
Returns Median, which is the time or voltage of the point at which 50% of the histogram is to the left or right (above or below for vertical histograms) as reported on the MHist Stats results table.