:MEASure:MHIStogram{N}:STDDev?

Query Syntax

:MEASure:MHIStogram{1:4}:STDDev?

Description

Returns Std Dev, which is the standard deviation of the histogram as reported on the MHist Stats results table.