:MEASure:PJITter:EOJ:STATus:DETails?
Query Syntax
:MEASure:PJITterN:EOJ:STATus:DETails?
Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.
Description
Returns a string that may provide additional details for a failed :MEASure:PJITter:EOJ? measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :MEASure:PJITter:EOJ:STATus:REASon? sibling query. Use the :MEASure:PJITter:EOJ:STATus? parent query to determine if the measurement has failed.