:MEASure:PJITter:JNU:STATus:REASon?

Query Syntax

:MEASure:PJITterN:JNU:STATus:REASon?

Where N identifies one of four possible PAM jitter analyses {1:4}. For example, PJITter4.

Query Response

Refer to the table "Common Reasons for INV or QUES Status".

Description

Returns a string that explains the reason for a failed :MEASure:PJITter:JNU? measurement. If the measurement was successful, a null string is returned.

Additional information about the failure may be available using the :MEASure:PJITter:JNU:STATus:DETails? sibling query. Use the :MEASure:PJITter:JNU:STATus? parent query to determine if the measurement has failed.

See Also