:MEASure:SNDRatio:RLMismatch
Command Syntax
:MEASure:SNDRatio:RLMismatch
Query Syntax
:MEASure:SNDRatio:RLMismatch?
Description
For PAM3 and PAM4 signal types (see :<source>:SIGNal:TYPE), the Ratio of Level Mismatch is a measure of the smallest separation between adjacent levels divided by the ideal separation.
When adding this measurement, the waveform on which measurements are made depends on the selected SNDR Standard (see :<source>:SNDRatio:STANdard).
| Standard | Standard Name | Waveform on which measurements are made |
|---|---|---|
| PCIe | PCIe | The selected Source input channel |
| IEEe | IEEE (PRBS13Q) | The SNDR Input waveform |
| IDJ | IEEE 802.3 dj | The SNDR Input waveform |
| ASA45 | ASA SG4, 5 | The SNDR Input waveform |
| Standard | Standard Name | Waveform on which measurements are made |
|---|---|---|
| USB4 | USB4 Gen 4 | The SNDR Input waveform |
SNDR measurement parameters are defined for the waveform source selected by :MEASure:SNDRatio:RLMismatch:SOURce.
Example Command Sequence
:MEASure:SNDRatio:RLMismatch:SOURce CHANnel1 :CHANnel1:SNDRatio:STANdard PCIe :CHANnel1:SNDRatio:PUINterval 32 :CHANnel1:SNDRatio:NAVerages 8 :CHANnel1:SNDRatio:LFPLength 600 :CHANnel1:SNDRatio:LFPDelay 8 :MEASure:SNDRatio:RLMismatch :MEASure:SNDRatio:RLMismatch?