:MEASure:SNDRatio:SNDRatio:STATus:REASon?
Query Syntax
:MEASure:SNDRatio:SNDRatio:STATus:REASon?
Query Response
Refer to the table "Common Reasons for INV or QUES Status".
Description
Returns a string that explains the reason for a failed :MEASure:SNDRatio:SNDRatio measurement. If the measurement was successful, a null string is returned.
Additional information about the failure may be available using the :MEASure:SNDRatio:SNDRatio:STATus:DETails? sibling query. Use the :MEASure:SNDRatio:SNDRatio:STATus? parent query to determine if the measurement has failed.