:MEASure:SNDRatio:SNPLevel:LEVel
Command Syntax
:MEASure:SNDRatio:SNPLevel:LEVel {LEVel0 | LEVel1 | LEVel2 | LEVel3}
Query Syntax
:MEASure:SNDRatio:SNPLevel:LEVel?
Description
Selects the level of a NRZ or PAM signal that will be measured when the :MEASure:SNDRatio:SNPLevel parent command is sent. NRZ signals have two possible levels: 0 and 1. PAM3 signals have three possible levels: 0, 1, and 2. PAM4 signals have four possible levels: 0, 1, 2, and 3.