:MEASure:USER:USER{N}:LSTatus:DETails?

Query Syntax

:MEASure:USER:USER{N}:LSTatus:DETails?

Description

If the status of the configuration file load is questionable or invalid (see :MEASure:USER:USER{N}:LSTatus?), this query returns a string that may provide additional details.

If the status of the configuration file load is valid, this query returns an empty string.

For a basic reason for the questionable or invalid status, use the :MEASure:USER:USER{N}:LSTatus:REASon? sibling query.