:MEASure:VERTical:VPP:UREFerence:STATe

Command Syntax

:MEASure:VERTical:VPP:UREFerence:STATe {ON | OFF | 1 | 0}

Query Syntax

:MEASure:VERTical:VPP:UREFerence:STATe?

Query Response

{1 | 0}

Description

Enables or disables a user-defined horizontal reference location near which a one-measurement-per-acquisition measurement is made.

When a user-defined horizontal reference location is enabled, the :MEASure:VERTical:VPP:UREFerence:VALue command specifies its time location with respect to the trigger (t = 0) location.