Skip To Main Content
  • placeholder
Filter:
Submit Search
You are here:

:MEASure:VERTical:VRMS:LOCation?

Vrms Commands
  • :MEASure:VERTical:VRMS
  • :MEASure:VERTical:VRMS:AREA
  • :MEASure:VERTical:VRMS:EDIRection
  • :MEASure:VERTical:VRMS:FAVorite
  • :MEASure:VERTical:VRMS:LOCation?
  • :MEASure:VERTical:VRMS:REGion
  • :MEASure:VERTical:VRMS:SOURce
  • :MEASure:VERTical:VRMS:STATus?
  • :MEASure:VERTical:VRMS:STATus:DETails?
  • :MEASure:VERTical:VRMS:STATus:REASon?
  • :MEASure:VERTical:VRMS:TYPE
  • :MEASure:VERTical:VRMS:UREFerence:STATe
  • :MEASure:VERTical:VRMS:UREFerence:VALue

PAM Waveform?

Use this command instead:

  • :MEASure:PAM:RMS:LOCation?

Query Syntax

:MEASure:VERTical:VRMS:LOCation?

Description

Returns an index for the location of the VRMS measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.