:MEASure:VERTical:VTIMe:TIME
Command Syntax
:MEASure:VERTical:VTIMe:TIME<time>
<time> is a double.
Query Syntax
:MEASure:VERTical:VTIMe:TIME?
Description
Specifies the time at which the Amplitude-at-Time measurement is made. Use the :MEASure:VERTical:VTIMe to make the measurement.
Example Command Sequence
:MEASure:VERTical:VTIMe:SOURce CHAN1_1 :MEASure:VERTical:VTIMe:TIME 200E-12 :MEASure:VERTical:VTIMe :MEASure:VERTical:VTIMe?