:SNOise:CALibrate:CONTinue
Command Syntax
:SNOise:CALibrate:CONTinue
Description
This command continues or proceeds to the next step of the oscilloscope noise calibration. For example, the calibration will prompt you to disconnect inputs to the channel being calibrated, and you would send this command after the inputs have been disconnected, in order to continue with the calibration.
This command is the same as clicking the Continue or Next buttons in the graphical user interface.