:SYSTem:ERRor:COUNt?

Query Syntax

:SYSTem:ERRor:COUNt?

Description

Returns the string which is the number of errors contained in the error-message buffer. To return the "first in" error, use the :SYSTem:ERRor:NEXT? query.

Example Python 3 Script

This script opens a session with Infiniium 2026 running on the PC and sends two invalid commands that create two error messages. Infiniium 2026's error buffer is then queried for the errors.

import pyvisa  # PyVISA package

rm = pyvisa.ResourceManager()
Infiniium = rm.open_resource('TCPIP0::localhost::hislip0,4880::INSTR') #HiSLIP

Infiniium.timeout = 20000 # Set connection timeout to 20s
Infiniium.read_termination = '\n'
Infiniium.write(':HAPPY:BIRTHDAY TODAY') # Illegal command for error!
Infiniium.write(':TIMebase:POSition 2.4E10') # out of range for error!
error_cnt = int(Infiniium.query(':SYSTem:ERRor:COUNt?'))
if error_cnt == 0:
    print('\n\tNo Infiniium errors reported.')
else:
    for i in range(0,error_cnt):
        print(f'\tERROR: {Infiniium.query(":SYSTem:ERRor:NEXT?")}')
Infiniium.write(':SYSTem:GTLocal')
Infiniium.close()