:TRIGger:SEQuence:EDGE:SLOPe
Command Syntax
:TRIGger:SEQuence{A|B}:EDGE:SLOPe {POSitive | NEGative | EITHer}
Query Syntax
:TRIGger:SEQuence{A|B}:EDGE:SLOPe?
Description
In the Edge trigger mode (see :TRIGger:SEQuence:MODE), this command specifies the edge of the Trigger Source (see :TRIGger:SEQuence:EDGE:SOURce) that will trigger.