:TRIGger:SEQuence:TIMeout:MODE
Command Syntax
:TRIGger:SEQuence{A|B}:TIMeout:MODE {HTLong | LTLong | UTLong}
Query Syntax
:TRIGger:SEQuence{A|B}:TIMeout:MODE?
Description
In the Timeout trigger mode (see :TRIGger:SEQuence:MODE), this command specifies the type of timeout:
HTLong— Triggers when the waveform is above the threshold level for longer than the specified:TRIGger:SEQuence:TIMeout:TIME(High Too Long).LTLong— Triggers when the waveform is below the threshold level for longer than the specified:TRIGger:SEQuence:TIMeout:TIME(Low Too Long).UTLongn— Triggers when the waveform has not crossed the threshold level for longer than the specified:TRIGger:SEQuence:TIMeout:TIME(Unchanged Too long).