:WAVeform:XYFormat:POINts?
Query Syntax
:WAVeform:XYFormat:POINts?
Description
Queries the record length (number of points) in the waveform's XYFormat data. Use :WAVeform:SOURce to select the source waveform. On a waveform acquisition, data can be missing in one of the following situations:
- When equivalent-time sampling is used, occasionally data may be missing on a few points.
- When an entire waveform pattern is being acquired and the acquisition has not yet completed.