Messages

Instrument messages are displayed in the message log which you can view by clicking the message log icon. Many of the messages can also be remotely queried using the :SYSTem:ERRor:NEXT? command. Messages provide information about the status of the instrument or an action that has been performed (for example, Calibration is complete). Messages also appear to inform you of errors that may have occurred. The following icons may be present to indicate the message type:

Operational error messages indicate instrument hardware or software failures. This type of message will remain on the display until the error condition is corrected.

Advisory messages allow you to take a recommended action. This type of message indicates if an operation did not complete or was cancelled.

Informational messages provide instrument status messages. No action is required.

If the Message Area is not displayed, click Setup > Display... to open the Display Setup dialog box. Select the Appearance tab and select Dock Message Area.

Messages

The messages included in the following table can be reported on the display or remotely returned.

Number Message
-NNN <description_string>. See: Negative-Numbered Messages
2 Could not send to socket
10 setting is at limit
11 setting is set to limit: Entry was out of range
12 Item entry was not a valid selection
13 file is disabled
14 The operation was not completed. The instrument is busy or not responding.
15 Item entry was limited to count characters.
16 Invalid character(s) removed from file entry
17 ".file" is not a valid extension for count. Using extension ".{2}".
18 Invalid filename: file
19 item must have at least count values
20 item cannot have more than count values
21 All functions in use. Please delete some functions and try again.
22 All {0} windows in use. Please remove a {0} window and try again.
23 All S-Parameter/Transfer Function Viewer files in use. Please clear a file in the Viewer and try again.
24 There is no valid frequency data. Check input signal.
25 All {0} traces are in use. You must uncheck some signals before more traces can be used.
26 No setup options selected.
30 Unable to read from signal item.
31 Unable to write to signal item.
40 item has recovered from an unexpected software problem.
41 item is busy or not responding.
42 Out of memory. Restart the application as soon as possible.
43 Insufficient memory to process item. Reduce the record length or turn off some signals.
44 This feature is not currently supported.
45 Unable to access the clipboard.
46 {0} Restart the application as soon as possible.
47 Image capture failed; move application to foreground and retry.
49 File does not exist at '{0}'
50 Characterizing Edges… percent complete
51 Unable to Characterize Edges: item
54 Parameter changed: Perform Auto Scale to resume measurements
55 Jitter measurements cannot be performed item
58 Characterizing Uncorrelated Jitter...
61 Acquisition stopped. item limit reached.
62 Acquisition timed out. Please provide a suitable trigger signal item.
63 Acquisition Failed: {0}
75 Please wait for the instrument to reach operating temperature...
79 The instrument has reached operating temperature.
80 Incompatible file: Cannot load item into item.
83 Unknown file format or version.
84 Unable to save: item
85 Unable to load due to insufficient memory.
86 A serious problem has occurred while loading/saving a memory.
87 File is corrupt: item
90 Invalid measurement detected.
91 file is not a recognized measurement.
92 The item measurement is not specified correctly.
93 Please turn on a valid source for the measurement measurement.
94 Screen too small: Infiniium has been scaled to fit this screen.
95 Custom DPI scaling detected (item%): count
99 Please enable a region for the measurement measurement.
100 The remote item did not respond.
101 The connection to the remote item has been lost.
102 An unexpected remote item communication error occurred: item
107 Connected to: item
108 Unable to connect: item
110 Waveforms are restricted in length to file
112 A file has not been selected for the name operator driving math function
118 The interpolation factor was restricted to item because waveform length is restricted to count
119 Unable to normalize: item
120 Unable to write to file "item"
121 Unable to read from file "item"
122 Could not load "item": item
125 File save complete: "item"
126 File read complete: "item"
127 Preset "name" saved successfully.
128 Preset "name" loaded successfully.
131 Creating transfer function...
132 Saved "file"
140 Autoscaling...
141 Autodetecting parameter...
142 Calculating Channel Scales...
143 Autoscale: message
144 Autoscale: message
145 Autodetection: item
150 Error loading mask file: …
151 Unrecognized command in mask file: file
152 Invalid argument argument for setup command: command
153 Missing mask margin definition for region number
154 Queries are not supported in mask file setup.
155 This mask file is not fully supported.
157 Mask file not specified.
160 Unable to start the License Manager.
161 Unable to find the License Manager. Verify that it was installed correctly and try again.
162 Unable to connect to the License Service.
163 The License Service is still initializing. This can take a few minutes.
164 License Service Error: {0}
165 Connected to the License Service for local licenses only.
166 The License Service is unavailable.
167 The feature {0} is unlicensed.
168 The License Service is unable to get the Host ID.
171 "item" was saved under a different configuration and may not have been completely restored.
174 The item SCPI server is running item.
175 The item SCPI server could not be started item.
176 The item SCPI server is not running.
177 Measurement location index is out of range.
183 file has no valid data.
184 Calibration is required for item.
185 Probe Attenuation has been set to file for count
191 All 64 functions have been configured. Remove a function before configuring a new one.
195 All Measurement Histograms in use, Please remove one and retry
196 Please turn on an FFT signal for the {0} measurement.
197 Please turn on a real-time eye signal for the {0} measurement.
210 file
220 No valid waveform data.
221 Could not compute symbol rate: {0}.
222 Too few edges found in waveform. Adjust the thresholds or acquire more data to compute the symbol rate.
240 Connected to: file
241 Unable to connect: device
242 New devices have been detected.
243 Incorrect Symbol Rate or Pattern Length specified for file file.
245 item used address address.
250 Unexpected error in external application description file item, line count.
251 Unexpected error launching external application item.
252 file is not a registered external application.
253 The external application description file item is incomplete.
261 Instrument Adjustment is required.
264 The instrument at connection number does not have a valid digital signature and may be a counterfeit.
266 The file device FPGA firmware is obsolete. Please reprogram the FPGA to version count or later.
280 general message
281 item
282 Error loading "target": explanation.
283 Could not find element "item". Make sure this file is for a count.
284 Error loading "{0}": File must be on a local hard drive.
285 Multiple entries of the same dependency "{0}".
296 Cannot create memory: source does not contain S-Parameter data.
297 Error loading S-parameter file: item
298 The loaded S-parameter file does not use standard differential port mapping.
299 This BETA version of application has expired. Please upgrade to a supported version.
300 Unable to set permissions on "file"
310 Unable to load limit line file: "file"
311 Limit line test created from a clipped waveform.
330 The item module has corrupt contents. Recovery may be possible.
336 Overload detected on item! Infiniium changed the vertical scale and/or offset.
338 {0} is outside of the calibrated temperature range. Measurements may not be accurate.
339 Overload detected on {0}! Disconnect the input immediately to avoid hardware damage.
371 The instrument user data partition does not exist. Please contact Keysight support.
372 Invalid input for parameter '{0}': {1}.
373 {0} {1} found on {2}.
374 No {0} found on {1}.
375 No acquisition data available to force qualify.
376 The input is already qualified.
377 The selected measurement has no data.
378 {0} was limited to {1} because {2} is using extended timer resources.
390 Initializing Hardware ...
391 Hardware Initialization Error: {0}
392 External 10 MHz reference not found. Infiniium has reverted to the internal reference.
393 The internal reference clock has failed to initialize. Contact Keysight Support.
394 External 8 GHz reference not found. Check the clock source and relaunch Infiniium.
396 Switching to the {0} 8 GHz reference...
397 The requested vertical scale could not be achieved due to a hardware problem. Contact Keysight Support.
400 Probe detected on {0}. It may take some time to initialize.
401 {0} is initialized on {1}.
402 Probe removed from {0}. Wait 10 seconds before connecting that probe to any channel.
403 Unable to communicate with probe on {0}. Power cycle the oscilloscope.
404 Unable to communicate with probe on {0}.
405 Probe on {0} has encountered a firmware error.
406 Probe on {0} is not supported by this instrument and/or software.
407 Probe on {0} is not supported due to an impedance mismatch.
408 Probe on {0} is not supported due to a coupling mismatch.
409 Oscilloscope Optimization Module on {0} is not supported on this instrument. Please use the following module(s): {1}.
410 Probe power supply failure detected on {0}. Resetting the probe now. This may take some time.
430 VTerm over-current detected on {0}.
431 VTerm over-temperature detected on {0}.