Adding Parameters to a Command

Many commands have parameters that require an argument. Use a space character to separate the argument from the command as shown in the following line:

:TIMebase:SCALe 100E-6