Copy Setup From Channel

In the channel Setup dialog box, the Copy From... button lets you copy settings from a different channel. Copied settings include the following:

  • Scale
  • Offset
  • Hardware Skew
  • Software Delay
  • Signal Type Auto Detect and Type
  • External Transducer settings
  • External Attenuator settings

The copied settings do not include waveform color or any custom waveform name.