Infiniium 2026 User's Guide
For real-time oscilloscope products
This online help describes the Infiniium 2026 application that is the Graphical User Interface (GUI) for the Infiniium XR8 real-time oscilloscopes. The same application, called Infiniium 2026 Offline, can be installed on a PC and used to view captured and saved oscilloscope data or data from simulated instruments.
Whether Infiniium 2026 is running on an oscilloscope or a PC, it can be controlled from a remote computer over LAN or USB via its SCPI interface. This is described in the Infiniium 2026 Programmer's Guide online help.
The following picture shows the Infiniium 2026 ecosystem where these connections and setups are possible.