Edge Direction
The Edge Direction option lets you select between Rising, Falling, or Both. Typically, for all clock recovery methods except Explicit, you would use Both edges of a signal to recover a clock. However, the other options are available if, for example, the signal is a clock signal with a low duty cycle and you want to measure jitter only on its rising (or falling) edges.
This option does not apply to PAM type signals.