Dialogs
Dialog Opacity and Transparent Background
You can select the Transparent Background check box which displays dialog box backgrounds that allow you to view any underlying waveforms. Use the Dialog Opacity setting to control the amount of transparency that is applied to dialog boxes.
Dialog Size
You can select small, normal, or large dialog boxes using the Dialog Size drop-down list. The default size is normal.