Normal (non-zoomed) Mode or Full-Screen Zoomed Mode
Use the scaling button, located at the bottom of the dialog box, to set the Infiniium's window size. The button goes to Full-Screen Zoomed Mode or Normal (non-zoomed) Mode, which is the default setting.
Full-zoomed mode formats the display for improved viewing when making presentations on a large screen. On the oscilloscope, you can connect a second, large display to the rear-panel connection.