Show Timebase Status Button

When the Show Timebase Status Button is selected, the large Horizontal status button/badge is located next to the channel bar as shown in the following picture. This is the default setting.

Clearing this selection removes the Horizontal badge to allow more room for the channel bar. A smaller Horizontal button is placed between the channel bar and the graticule as shown in the following picture.