Screen/Pen/Touch Calibration

Screen/Pen/Touch calibration aligns the XY positions on touchscreen or mouse with the a display. The oscilloscope does not provide its own calibration application. Instead, exit the Infiniium graphic interface and use the Windows start menu to search on "screen calibrate" or "touch" to locate the calibration application. If you have installed a custom mouse or pen pad, the manufacturer of the device may provide its own calibration application.