BIN File Format
BIN (.bin) format files contain headers and data in the following order:
-
File Header — There is only one file header in a binary file. The file header contains these fields:
- Cookie — Two byte characters, AG, which indicates that the file is in the Keysight Binary Data file format.
- Version — Two bytes that represent the file version.
- File Size — An integer that is the number of bytes that are in the file.
- Number of Waveforms — An integer that is the number of waveforms stored in the file.
After the File Header, for each waveform, there is this order:
- Waveform Header — The waveform header contains information about the type of waveform data that is
stored following the waveform data header, which is located after each waveform
header. Because it is possible to store more than one waveform in the file, there
will be a waveform header and a waveform data header for each waveform. The waveform header contains these fields:
- Header Size — An integer that is the number of bytes in the header.
- Waveform Type — An integer that is the type of waveform stored in the file. The following list
shows what each value means:
- 0 = Unknown
- 1 = Normal
- 3 = Average
- 4 = Horizontal Histogram
- 5 = Vertical Histogram
- 6 = Logic
- Number of Waveform Buffers — An integer that is the number of waveform buffers required to read the data.
- Points — An integer that is the number of points in the waveform.
- Count — An integer that is the number of hits at each time bucket in the waveform record when the waveform was created using an acquisition mode like averaging. For example, when averaging, a count of four would mean every waveform data point in the waveform record has been averaged at least four times. Count is ignored when it is read back into the oscilloscope. The default value is 0.
- X Display Range — A float that is the number of X display range columns (n) depends on the number of sources being stored. The X display range is the X-axis duration of the waveform that is displayed. For time domain waveforms, it is the duration of time across the display. If the value is zero then no data has been acquired.
- X Display Origin — A double that is the number of X display origin columns (n) depends on the number of sources being stored. The X display origin is the X-axis value at the left edge of the display. For time domain waveforms, it is the time at the start of the display. This value is treated as a double precision 64-bit floating point number. If the value is zero then no data has been acquired.
- X Increment — A double that is the number of X increment columns (n) depends on the number of sources being store. The X increment is the duration between data points on the X axis. For time domain waveforms, this is the time between points. If the value is zero then no data has been acquired.
- Y Origin — A double that is the number of X origin columns (n) depends on the number of sources being store. The X origin is the X-axis value of the first data point in the data record. For time domain waveforms, it is the time of the first point. This value is treated as a double precision 64-bit floating point number. If the value is zero then no data has been acquired.
- X Units — An integer that is the number of X units columns (n) depends on the number of
sources being store. The X units is the unit of measure for each time value of the
acquired data. X unit definitions are:
- 0 = Unknown
- 1 = Volt
- 2 = Second
- 3 = Constant
- 4 = Amp
- 5 = Decibel
- Y Units — An integer that is the number of Y units columns (n) depends on the number of
sources being stored. The Y units is the unit of measure of each voltage value of
the acquired waveform. Y units definitions are:
- 0 = Unknown
- 1 = Volt
- 2 = Second
- 3 = Constant
- 4 = Amp
- 5 = Decibel
- Date — A 16-character array that is the date when the waveform was acquired. The default value is 27 DEC 1996.
- Time — A 16-character array that is the time when the waveform was acquired. The default value is 01:00:00:00.
- Frame — A 24-character array that is the model number and serial number of the oscilloscope in the format of MODEL#:SERIAL#.
- Waveform Label — A 16-character array that contains the label assigned to the waveform.
- Time Tags — A double that is the time tag value of the segments being saved.
- Segment Index — An unsigned integer that is the segment index of the data that follows the waveform data header.
Then, for each waveform buffer within a waveform, there is this order:
- Waveform Data Header — The waveform data header consists of information about the waveform data points
that are stored immediately after the waveform data header. The waveform data header contains these fields:
- Waveform Data Header Size — An integer which is the size of the waveform data header.
- Buffer Type — A short which is the type of waveform data that is stored in the file. The
following shows what each value means.
- 0 = Unknown data
- 1 = Normal 32 bit float data
- 2 = Maximum float data
- 3 = Minimum float data
- 4 = Time float data
- 5 = Counts 32 bit float data
- 6 = Digital unsigned 8 bit char data
- Bytes Per Point — A short that is the number of bytes per data point.
- Buffer Size — An integer that is the size of the buffer required to hold the data points.
- Waveform Data — The data for the waveform buffer.
An example program of reading BIN (.bin) format files is at: binary-to-csv.py