Save Protocol Files

When you have used protocol decode on captured data, you can save the packet decode information to a file.

Use the Source selection to specify the protocol decode from which to save.

Use the Listing selection to specify the symbol listing or packet listing from which to save.

Use the File Type selection to specify the format of the output file:

  • All protocol decodes can be saved in the comma-separated value (*.csv) format.