Align Operator

The Align math operator lines up two single-values waveforms or eye diagrams. Time delay is applied to the top operand to move it reference to the bottom operand. To align the two waveforms, click on the operator icon which opens the dialog box shown in this figure. If the Automatic Align does not meet your needs, clear the check box and manually enter the time delay.

Input Waveforms Before Align

Waveforms After Align

Display Setup

Each operator's setup includes a Setup section that has the selections that are shown in the following generic setup dialog box. Use these settings to control the display of the operator's output waveform, including turning the display on or off. Use the Name field to display an identifying name to the waveform which can be helpful for screen captures or when multiple waveforms are displayed. The settings also include the output waveform's color, scaling, and signal type. The scaling Automatic selection allows the output waveform to track changes to the scaling of the input waveform. This is the setting that you would normally want to use.

The signal Pattern can be used for BER (Bit Error Ratio), SNDR (Signal to Noise and Distortion Ratio), and other measurements. You can specify the math function has the same pattern as the input waveform (Track Input), Auto Detect the pattern, choose a Known Pattern from a list, or specify your own pattern using a Pattern File.