FFT Peak Detection

  • Enable — When checked (enabled), the first N peaks in the FFT above the specified Peak Level are annotated. N is specified by the Max Peak Count control.

    The annotated peak values are displayed in the FFT Peaks panel.

    The peak level appears as a numbered marker in the FFT window.

  • Peak Sort — Specifies whether peaks are annotated by Decreasing Magnitude, Increasing Frequency, Decreasing Frequency, or Increasing Magnitude order. Peak annotations are numbered according to the chosen sort.

  • Max Peak Count — Specifies the number of peaks in the FFT to annotate.

  • Peak Level — The level above which peaks are identified.

  • Peak Excursion Level — Specifies the amplitude above the FFT waveform's noise floor necessary to be recognized as a peak.