<Enumeration> Element

The <Enumeration> element adds a User-Defined Control to the User Operator Setup dialog box. The type of control is an drop-down list. You can select one item from many selections as shown in the picture below. Selections in the drop-down list are arranged in the order of the <Selection> child elements in the XML file. A maximum of 10 selections can be defined. In order for your script to access this setting, the "Name" attribute in the parent <Control> element must be the name of a string script variable.

Do not use spaces or hyphens when naming your user-defined controls.

  • <Control Name = "FilterType">
  • <Enumeration>
  • <Default>lowpass</Default>
  • <Selection>highpass</Selection>
  • <Selection>low</Selection>
  • <Selection>bandpass</Selection>
  • </Enumeration>
  • </Control>

Parent Elements

Child Elements

Attributes

None

Example

  • <Function>
  • <Control Name = "Selections">
  • <Enumeration>
  • <Default>Medium</Default>
  • <Selection>High</Selection>
  • <Selection>Medium</Selection>
  • <Selection>Low</Selection>
  • </Enumeration>
  • </Control>
  • </Function>