<Max> Element

The <Max> element establishes the maximum value that can be entered into a <Integer> or <Double> User-Defined Control data-entry field. Use the <Min> element to establish the minimum value.

Parent Elements

Child Elements

None

Attributes

None

Example

  • <Function>
  • <Control Name = "Fc">
  • <Double>
  • <Min>10e6</Min>
  • <Max>1000e9</Max>
  • <Resolution>1000</Resolution>
  • <Units>Hertz</Units>
  • <Default>7.5e9</Default>
  • </Double>
  • </Function>