USB Ports

The front panel includes two USB 3.0 Type A ports, which are provided for devices such as a keyboard or external memory.

Each front-panel port provides power for devices such as pen drives, which you can use to save and load setups, waveforms, and screen images to and from the instrument's hard disk.

Additional USB ports are on the rear panel.

The rear panel includes the following USB ports:

  • One USB 3.0 Type B ports
  • Two USB 3.0 Type A ports
  • Two USB 2.0 Type A ports