<Setup> Element

The child elements of the <Setup> element configure settings in the Mask Test Scaling dialog box as shown by the following figure. The child element <MaskAlignmentOptimize> does not have an equivalent dialog box setting.

Figure. Elements for Mask Test Scaling Dialog Box

If you do not define a mask setup section in your mask file, the setup data from the last mask that was loaded will be used. This could cause unexpected or erroneous positioning of the mask.

Parent Elements

  • <Mask>

Child Elements

Attributes

None.