Ratio of Level Mismatch
For PAM3 and PAM4 signal types, the Ratio of Level Mismatch is a measure of the smallest separation between adjacent levels divided by the ideal separation.
When adding this measurement, the waveform on which measurements are made depends on the selected SNDR Standard:
| Standard | Waveform on which measurements are made |
|---|---|
| PCIe | The selected Source input channel |
| IEEE (PRBS13Q) | The SNDR Input waveform |
| IEEE 802.3 dj | The SNDR Input waveform |
| ASA SG4, 5 | The SNDR Input waveform |
| Standard | Waveform on which measurements are made |
|---|---|
| USB4 Gen 4 | The SNDR Input waveform |
SCPI Command
:MEASure:SNDRatio:RLMismatch