Sigma-n Per Level
Sigma-n Per Level is a measurement of noise on the flattest portion of consecutive symbols, for each symbol level, according to the selected standard.
Sigma-n is an averaged measurement of the RMS deviation from the mean voltage noise (σ) at all signal levels. It represents essentially the crosstalk and all other external noise.
The Sigma-n measurement computes the noise parameter, σn, for waveforms according to the selected technology standard. The parameter σn measures the uncorrelated RMS amplitude noise of each symbol level (including random noise and bounded uncorrelated noise effects), while not including ISI (inter-symbol interference) and jitter effects.
SCPI Command
:MEASure:SNDRatio:SNPLevel