PAM Level Skews
The PAM Level Skews measurement measures the skew (seconds or UI) of each level of a PAM eye diagram relative to the average center time of all levels. On NRZ signals, this measurement will measure the level one and zero skew relative to each other.
| Setting | Description |
|---|---|
| PAM-N Analysis Setup Dialog Box Settings | |
| Receiver Sample Timing | Configures the timing for sampling the signal data for all PAM measurements. |
| Eye Center Location | Selects the basis for determining the location of an eye's center on the waveform: at maximum eye width or maximum eye height. |
| Eye Level Width | Defines the timespan (in percentage of symbol width) over which an eye's amplitude level is measured. |
| Time of Level | Specifies the method used to locate the time at which to measure an eye's level. |
| Time Units | Sets the time units for measurement: seconds or unit intervals. |
The skew of each level is calculated by:
- For each level, determine the time at which the level's thickness is at a minimum value. The minimum value is determined by minimum RMS or peak-to-peak values (Level Time Method setting).
- Calculate the average time for all levels measured in step 1.
- Skew for each level is the time of the level calculated in step 1 relative to the average time calculated in step 2.
- Display the measurements in the units specified in the Time Units setting.
This measurement can be applied to both PAM and NRZ waveforms.
To measure
- Click Auto Scale in the menu toolbar.
- Click the measurement toolbar's PAM tab.
- On the toolbar, locate and click the Level Skews button.
SCPI Command
:MEASure:EYE:PAM:SKEW