Scaling the Phase Noise Analysis Display

To scale the phase noise analysis display:

  1. In the Phase Noise Setup dialog box, select the Display tab.

  2. To adjust the horizontal scale, edit the X Start and X Stop values.

  3. To adjust the vertical scale, edit the Y Scale and Y Offset values.